AXIS#.PL.MODPEN

Description

A value of 0 disables the modulo-position and a value of 1 enables the modulo-position feature. The modulo-position feature can be used for circular applications such as round tables.

The position loop of the drive uses a linear position variable but the data-exchange between the user and the drive uses the modulo-position calculation in order to convert values from linear format into modulo format and vice versa.

The following figure shows the interface between the user and the drive for AXIS#.PL.MODPEN=1:

Examples

Code

Axis 1 position is modulo’d to 0-360 where MODP1 is beginning of range and MODP2 is the end of range.

-->AXIS1.PL.FB
500.000 [deg]
-->AXIS1.PL.MODP1 0
-->AXIS1.PL.MODP2 360
-->AXIS1.PL.MODPEN 1
-->AXIS1.PL.FB
140.000 [deg]

Context

For more information see Modulo Position .

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AXIS#.PL.MODP1, AXIS#.PL.MODP2

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.MODPEN

500ch

0bh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5912

1

5912 (0x1718)

AXIS1.PL.MODPEN

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.MODPEN

5912

Unsigned8

Read/Write

-